Silicon Photonics

This blog post is part of a series called “CommScope Definitions,” in which we will explain common terms in communications network infrastructure.

Silicon photonics (SiPh) is a technology that involves data being transferred among computer chips by optical rays. On the surface, it seems simple, but it can actually be difficult to understand. Perhaps it is best to compare it to an electrical circuit. 

In the early days of electrical circuits, there were discrete components (e.g., transistors, capacitors, resistors, etc.) that were connected with traces on a printed circuit board.  In order to reduce size and cost, many discrete components were formed adjacently and interconnected on a single silicon substrate to create integrated circuits (i.e. chips).  Over time, the types of components that could be formed on chips continued to expand while their size and power consumption shrank at dramatic rates (per Moore’s law).  We now have billions of interconnected components per chip, each at a negligible cost.

The objective of silicon photonics is to enable the same cost effective component integration in the optical domain.  Specifically, optical components (e.g. lasers, splitters, modulators, combiners, etc) are interconnected with transparent pathways or waveguides for light to travel through, much like electricity runs through traces on a circuit board.  The industry has focused on leveraging the investments made in silicon by the electrical chip industry wherever possible.  

SEE ALSO: Silicon photonics market to grow 21% from 2016 to 2022

Although the technical capability of SiPh has continually progressed, two related challenges have kept the cost of SiPh solutions high: 

  • It is not possible to form lasers directly in silicon. Instead, lasers are made out of other materials, and their output (light) is coupled into the waveguides. 
  • SiPh waveguides are small, making interconnections to and from the chips difficult and expensive.  Specifically, SiPh waveguides are less than half a micron in diameter which is about 1/20th the diameter of today’s standard single mode fiber.  Various alignment techniques are available, but they are expensive. 

An approach that is having significant market impact is to replace the pure silicon substrate with silicon dioxide (i.e., glass).  The resulting circuit is called Photonic Light Circuit (PLC).  The types of components that can be formed on PLCs is limited, but the use of glass substrates allows six times larger waveguides which reduces the alignment challenges to other components like lasers.  The combination of technologies is helping solve challenges and driving down the cost of high speed photonics.  It also redefines the industry’s direction from purely “silicon photonics” to the wider field of “integrated photonics.” CommScope tracks these developments closely as they impact the optimal choice of fiber type in multiple markets we serve.

Are you seeing intriguing developments around integrated photonics?  Comment here, and we’ll have a discussion that will keep all of us up to date with architectural advancements in this exciting field. 

About the Author

Luc Adriaenssens

Luc Adriaenssens is senior vice president of technology for CommScope in Richardson, TX.  He is focused on long-range strategic growth plans including technology focused equity investments and acquisitions.  His prior assignment was heading up CommScope’s Enterprise R&D division driving the R&D of copper, fiber and associated software solutions. Luc started his career in 1986 as a cable designer at Bell Labs.  He has been involved with high performance cable & connector design, LAN cabling standards, cabling system applications, EMC testing, intelligent building platforms and product management.  He is an expert on cabling performance issues and was instrumental in shaping Category 5 cable and Category 6/6A cabling requirements.   He is the lead inventor of the multi-stage copper connector compensation method, delivering unrivalled channel performance. Luc hold BSEE, MSEE and MBA degrees from Georgia Tech, U.C. Berkeley and Purdue respectively.  Patents on which he is the lead inventor have grossed tens of millions of dollars in royalties.

See all posts by this author

Comments

2 comments for "CommScope Definitions: What is Silicon Photonics?"
Sukhi Friday, August 05, 2016 11:15 AM

A great article on what really is a new and upcoming technology, which is really starting to be embraced now. We organise a conference on photonic integrated circuits, www.picinternational.net. I would love to talk to someone from Commscope about having a presence at our conference and indeed speaking at the conference.

Luc Adriaenssens Tuesday, August 09, 2016 10:04 AM

Sukhi: Thanks for the feedback and conference tip. We’ve looked into the conference and do plan to have someone attend. There are some very good speakers on the agenda, many of which we have worked with before so appreciate the tip.

Add Your Comment

Please submit your comment using the form below

 
(required)