It is becoming a widely known fact in the cabling industry that patch cords can be the “weak link” in an end-to-end infrastructure solution. Historically, many focused on cable performance when making infrastructure decisions. However, connectors and patch cords have become significant contributors as cabling systems have evolved. Fine ‘tuning’ of these high performance components to each other, as well as variation control techniques, are required to enable reliable, predictable performance every time.

Testing of installed cabling has gained wide acceptance as a performance checking mechanism, and the technology has advanced to the point where testing up to 500 MHz is routinely performed quickly and accurately in the field. However the most widely used test configuration, the Permanent Link, was developed in standards to verify the performance of the installed link from patch panel to work area outlet. In other words, it specifically excludes the patch cords

Most customers assume that the addition of ‘standard compliant’ cords will guarantee the delivery of the required end to end performance. Why would they think otherwise? How can such a simple looking, off-the-shelf product make a difference?

Significant strides have been made to cabling standards over the years to specify requirements for components intended to deliver the expected end to end performance even in a mix-and-match environment. However I believe it is important to note that the standards specify minimum requirements only, and do not cover all the coupling and reflection effects that may occur within or between components. In addition and as highlighted by an excellent blog post by Jim Hulsey (You get what you pay for), ‘standards compliance’ is a self certification which means anyone can make the claim, it is up to the customer to believe them. 

Designing patch cords to overcome the “weak link” concerns

A patch cord is constructed with flexible cordage and a modular (RJ45) plug on each end. In order to deliver optimal performance, the characteristics of the cordage are carefully matched to the plug, including jacket type, thickness and overall outer diameter, the orientation of the pairs at each end prior to termination, the twist rate, the insulation diameter, the conductor diameter, and many others. 

Poorly assembled plugs will deliver inconsistent performance and may exhibit intermittent continuity – a network manager’s worst nightmare! In extreme cases, badly assembled plugs may even damage the contact pins in cabling or switch ports, for example when the plug ‘blades’ are loose, too high or out of alignment.

The arrangement of each cable pair inside the plug must also be carefully controlled. This enables system vendors such as CommScope to tune jacks and plugs to achieve performance above the minimum standard requirements.

CommScope has developed highly advanced modeling techniques to optimize channel performance, as well as sophisticated electrical, mechanical and manufacturing techniques to minimize the performance impact and variation that can result from sub-optimal matching of patch cords to the rest of the system. The system warranties offered by CommScope provide customers with an assurance of long-term performance beyond the minimum requirements of standards, as well as coverage in the unlikely event of quality defects.

Therefore, using ‘just any’ patch cord in a system may not only degrade performance but may prove to be a costly mistake in the event of a system failure, that may have been otherwise covered by warranty.

About the Author

James Donovan

James Donovan is Vice President of the CommScope Infrastructure Academy. James joined CommScope in 1993 and has held positions in Sales, Technical, Marketing, Training and Business Development and served most recently as VP of Digital and Creative Services for CommScope. James oversees the CommScope Infrastructure Academy, which is CommScope’s partner and customer training platform. Prior to joining the company, he held positions at GEC, ITT and Alcatel. He holds a Masters Degree in Engineering and a BSc Honors degree in Electrical and Electronic Engineering.

See all posts by this author

Comments

5 comments for "You Are The Weakest Link - Good Bye!"
James D Mitchell - the HelpMeCableGuy!

This is a great article, and especially timely with the counterfeit CCE Copper Clad Ethernet cables that have been sold as regular patch cords throughout the industry lately. I work for a website that sells many brands (including our own high-end brand) of patch cords; and we've seen many clients move away from making their own patch cords, and moving to pre-manufactured patch cables due to issues do to improper crimping or rushed cables. I'd go a step further and to say that, unless it's a necessity, it's better to use a pre-made patch cable than to try and make them yourself, in the field. Sure, you can do that, and yes, it will be fairly easy to do; but the savings (if any) is minimal and the possibility of a poor termination is greatly increased on site being made by hand, as opposed to a machined cable in a controlled factory environment. Great, informative blog post. I plan to forward this to my clients.

jamesdonovan

Thanks James, Let's hope the word gets out. Love the HelpMeCableGuy handle!

James D Mitchell - the HelpMeCableGuy!

Thanks James... the name came from relatives and friends asking me to "help them cable guy!" since I worked with cables and connectors all day long, and I used to answer a lot of questions on forums as the same handle. Plus, I loved the Jim Carrey movie... Also, I forgot to mention in the article: "I work for a website that sells many brands (including our own high-end brand) of patch cords; and..." I of course meant to say it this way: "I work for a website that sells many brands (including COMMSCOPE GigaSPEED and the SYSTIMAX Patch Cords and even our own high-end brand) of patch cords; and..." Thanks James!

jamesdonovan

And I thought I was the only one who is known by their friends and family to be a cable geek!

Blair Groves

Great article. Too many installs are done by un(der)-qualified individuals. As mentioned in another article, premise cable itself, as well as even more critical running to avoid EMI and proper termination and testing is all too often ignored by people who think they know it all. I've fixed too many botched installations, and yes, it is false economy to crimp your own patch cords. That's a key area where most know-it-all's fall flat on their faces - especially by terminating modular plugs directly to premise cable. The tools, materials and know-how is available to anyone, but just like electrical wiring or designing and coding a custom ERP system from scratch, you would hope everyone would know their limitations, and pay the true specialists to get correct results.

Add Your Comment

Please submit your comment using the form below

 
(required)