CommScope Expands Solutions to Support Wireless Operators’ Long-Term Strategies for Tackling Data Backhaul Challenges

--Alleviates Network Capacity Constraints and Saves Money where it Matters--
March 19, 2012 HICKORY, N.C.

Cellular providers have more options for handling the growing problem of network overload thanks to a ground-breaking microwave antenna solution from CommScope. Now, next-generation backhaul performance and savings in operating and capital expenses are within easy reach.

CommScope’s Sentinel™, one of the most significant innovations in Andrew Solutions™ microwave antenna technology, is designed to address three of the greatest challenges facing wireless network operators – rapidly increasing data traffic, spectrum scarcity and return on network investment. Sentinel is believed to be the first full line of European Telecommunications Standards Institute Class 4 antennas priced for today and designed for the future. And, CommScope believes Sentinel is the only offering of its kind that delivers these advantages without compromise.

Sentinel is engineered for performance to maximize the use of wireless spectrum, while withstanding heavy demands in data growth. As with all CommScope capacity solutions, customers benefit from added peace of mind knowing the technology powering their solution won’t become obsolete before or soon after deployment. An innovative improvement in radiation pattern helps squeeze more out of available spectrum and typically yields 40 percent higher link density. The result is more capacity moving traffic between cell sites and the core network, helping lessen strain on the network and prevent impacts to performance. Higher radio modulation schemes can be used and Sentinel can also minimize interference in the network.

Additionally, every component of the Sentinel solution is geared towards saving customers money. Consider how the price tag for a backhaul microwave antenna is really only part of the total overall cost of ownership – nearly 70 percent of the money spent on backhaul actually comes after the purchase. Sentinel allows smaller antennas to be deployed, which may provide savings in capital and operational expenses.

Bulkier-sized antennas drive up operating expenses due to larger tower space leasing and zoning considerations. Installations also are typically more complex and with greater maintenance requirements, which can increase the likelihood of longer network downtime. Sentinel’s small footprint makes installation easy and keeps maintenance costs low. The antenna is further designed to be lightweight yet durable, so it can endure winds as strong as 250 kilometers per hour (155 miles per hour).

“Wireless network operators are facing serious issues related to network capacity and with the rollout of LTE, traffic growth projections are expected to climb,” said Paul Bell, senior vice president of Microwave Antennas, CommScope. “There’s so much that needs to be factored into an effective backhaul solution, but it all comes down to performance and long-term costs. In creating Sentinel, as with all our other backhaul solutions, we wanted to give our customers the best of both worlds and something that would support them today and in the years ahead.”

Terrestrial microwave antennas produce highly directional beams typically used in point-to-point microwave systems. CommScope manufactures a full line of terrestrial microwave antennas for applications such as fixed-line telecommunications networks, broadband wireless, wireless infrastructure and television broadcasting. Our Andrew microwave antennas provide a cost-effective solution for all terrestrial microwave systems operating at frequencies between 3.5 GHz and 80 GHz and in sizes from 8 in. (0.2 m) to 15 ft. (4.6 m) in diameter.

About CommScope

CommScope (www.commscope.com) has played a role in virtually all the world’s best communication networks. We create the infrastructure that connects people and technologies through every evolution. Our portfolio of end-to-end solutions includes critical infrastructure our customers need to build high-performing wired and wireless networks. As much as technology changes, our goal remains the same: to help our customers create, innovate, design, and build faster and better. We’ll never stop connecting and evolving networks for the business of life at home, at work, and on the go.

This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

News Media Contact:
Camille Beasley, CommScope
+1 972-952-9780
publicrelations@commscope.com
or
Financial Contact:
Phil Armstrong, CommScope
+1 828-323-4848