CommScope Introduces New Angled Patch Panels

June 22, 2005 HICKORY, N.C.

CommScope, Inc. (NYSE: CTV), a world leader in cable and connectivity solutions, has added a new line of Angled Patch Panels (UNP500 and UNP600) to the Uniprise(TM) Solutions set for use in telecommunications rooms, equipment rooms and data centers. The patch panels are designed for quick and repeatable configuration of Category 5e and Category 6 circuits where rack space is limited and the customer requires a high density of patch capability.

"These new Angled Patch Panels are designed to eliminate the need for the cable management panel from the traditional layout," said Sandra Young, Global VP of Enterprise Marketing. "This allows more density in the rack by nearly doubling the number of ports available for use within the same footprint."

The panel backs consist of gas-tight insulation displacement connections for continuous metal-to-metal contact in the electrical connection, thus preventing the intrusion of air and moisture that can result in corrosion and failure. Patch cords can be routed directly into the vertical wire management patch cord organizers. Other features include a rear wire management/strain relief bar, labels and label holders. The UNP500 and UNP600 are available in 24- and 48-port versions.

CommScope launched the Uniprise brand of enterprise network solutions in 2004. The Uniprise product portfolio of end-to-end solutions encompasses Category 6, Category 5e, multimode fiber and singlemode fiber solutions. Uniprise offers a range of solutions designed to improve network performance and optimize connectivity needs. Its advantages include single-source convenience, one point of contact, product compatibility, superior quality control, performance guarantees and a comprehensive warranty.

CommScope is a world leader in the design and manufacture of 'last mile' cable and connectivity solutions for communication networks. Through our SYSTIMAX(R) Solutions and Uniprise brands we are the global leader in structured cabling systems for business enterprise applications and the world's largest manufacturer of coaxial cable for Hybrid Fiber Coaxial (HFC) applications. Backed by strong research and development, CommScope combines technical expertise and proprietary technology with global manufacturing capability to provide customers with high-performance wired or wireless cabling solutions.

This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. For a more detailed description of the factors that could cause such a difference, please see CommScope's filings with the Securities and Exchange Commission. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

Visit CommScope at our Web Site -- http://www.uniprisesolutions.com

"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995: Statements in this press release regarding CommScope's business which are not historical facts are "forward-looking statements" that involve risks and uncertainties. For a discussion of such risks and uncertainties, which could cause actual results to differ from those contained in the forward-looking statements, see "Risk Factors" in the Company's Annual Report or Form 10-K for the most recently ended fiscal year.

Tate Hoxworth of VantagePoint, Inc., +1-864-331-1289
or
Betsy Lambert of CommScope Media Relations, +1-828-323-4873
Web site: http://www.commscope.com
http://www.uniprisesolutions.com