CommScope, Inc. (NYSE: CTV), a world leader in cable and connectivity solutions, today introduced a new fiber optic Pavement Cable specifically designed to reduce installation costs and construction time. It can be used by MSOs to deploy fiber to commercial, residential and small-to-mid-sized businesses, and it is also designed for enterprise applications such as metropolitan and campus sidewalks, roadways and parking lots.
Available in up to 72-fiber count, CommScope's fiber optic pavement cable utilizes a gel-filled central tube cable encased in a smooth-wall, welded copper armor that provides it with enhanced fiber protection and water blocking characteristics. The product is rugged in design with excellent crush resistance and thermal stability while providing tensile performance compatible with standard micro-trenching techniques. Since sharp edges are minimized, it also provides fiber protection during cable access and termination.
The Pavement Cable's unique, patent-pending design allows an installation method that can substantially reduce disruption of day-to-day traffic at the installation site since it requires only a 10 mm wide by 8 cm deep groove to be cut into a sidewalk, roadway, or parking lot. The pavement cable is placed at the bottom of the slot and held in place by a closed-cell, foamed backer rod. The opening is then easily sealed with common, commercially available hot sealant, roofing tar or caulking, depending upon the surface.
"We believe our new pavement cable's installation method is a significant improvement over more costly and time-consuming directional boring and trenching techniques used in the past when an aerial installation of a fiber drop was impractical," said Brian Garrett, CommScope's President and COO. "Our fiber optic pavement cable is another example of our commitment to provide cost effective, commercial access solutions to our MSO and enterprise customers."
CommScope is a world leader in the design and manufacture of 'last mile' cable and connectivity solutions for communication networks. Through our SYSTIMAX(R) Solutions and Uniprise(TM) brands we are the global leader in structured cabling systems for business enterprise applications. We are also the world's largest manufacturer of coaxial cable for Hybrid Fiber Coaxial (HFC) applications. Backed by strong research and development, CommScope combines technical expertise and proprietary technology with global manufacturing capability to provide customers with high-performance wired or wireless cabling solutions.
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. For a more detailed description of the factors that could cause such a difference, please see CommScope's filings with the Securities and Exchange Commission. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Visit CommScope at our Web Site- http://www.commscope.com
Martin Lee, Product Mgr., Broadband Fiber, +1-828-431-2531
Steve Bailey, Product Manager, Network Fiber, +1-828-549-5731
Betsy Lambert, Media Relations, +1-828-323-4873, all of CommScope, Inc.
Web site: http://www.commscope.com