CommScope is offering a new, comprehensive antenna solution that enables wireless operators to significantly increase capacity at the cell site. The Six Sector Solution, part of the Andrew portfolio of wireless solutions, utilizes advanced antenna technology that can make site acquisition and installation easier by enabling the use of three antennas where six were previously needed. Implementation of the Six Sector Solution provides almost twice the capacity, increases the gain of each sector by 3 dB for better building penetration and mitigates interference for higher data throughput.

“The massive increase in subscriber demand for mobile data is driving a major concern among wireless operators about having enough capacity to handle the traffic,” said CommScope’s Philip Sorrells, vice president of strategic marketing, Wireless. “The Six Sector Solution is an excellent way to significantly increase capacity by enabling the evolution of a traditional three sector site to a higher capacity, six sector site with the use of only three antennas.”

The Six Sector Solution is the latest Andrew offering to address the concept of sector sculpting, a creative approach to antenna pattern shaping that carves out more capacity, improves coverage and limits interference. Sector sculpting boosts network performance by better controlling interference between sectors and increasing the number of accessible subscriber channels. These sector sculpting antennas, such as in the Six Sector Solution, can radiate multiple, tightly defined RF patterns from one antenna unit. Other Andrew sector sculpting offerings include the Five Beam, 18-Beam, UltraBand™ and SmartBeam® base station antennas. In addition, the Andrew Sentinel™ microwave backhaul antenna uses a similar pattern shaping approach to boost capacity between microwave links.

“In an era of limited spectrum and constantly increasing demands for bandwidth, CommScope strongly advocates the concept of sector sculpting as an effective way for operators to efficiently improve performance at their cell sites,” said Sorrells.

The Six Sector Solution utilizes twin beam base station antennas as the primary enabling technology for sector-splitting with three antennas. Twin beam antennas generate two RF beams from one antenna meaning three antennas can do the work of six, saving on tower leasing costs and decreasing wind loading. By increasing the gain in each sector by 3 dB, twin beam antennas nearly double the signal power, which means better building penetration. The higher gain also enables higher data rates so that customers may be able to stream high-definition videos, for example, where previously they could only stream low quality video. Twin beam antenna technology is now available in most frequency bands for GSM, CDMA, UMTS and LTE.

“We believe that increasing network capacity with a relatively simple antenna system upgrade is a great near term investment,” said Sorrells. “Our solution provides a practical way to quickly deploy sector-splitting without additional antenna faces.”

Adding further value, CommScope and its partners can offer North American customers turnkey design, planning and installation services with an overarching service warranty for the RF path as part of the Six Sector Solution. Similarly, CommScope expects to expand the Six Sector Solution into a complete product and services offering for customers in all regions of the world.

Related Blog Posts:

Are Your BSAs Ready for LTE-Advanced?
Channeling Mr. Spock – And Sector
A Sentinel Helps You Be Heard

SmartBeam is a registered trademark of CommScope, Inc. UltraBand and Sentinel are trademarks of CommScope, Inc.

About CommScope

CommScope (www.commscope.com) has played a role in virtually all the world’s best communication networks. We create the infrastructure that connects people and technologies through every evolution. Our portfolio of end-to-end solutions includes critical infrastructure our customers need to build high-performing wired and wireless networks. As much as technology changes, our goal remains the same: to help our customers create, innovate, design, and build faster and better. We’ll never stop connecting and evolving networks for the business of life at home, at work, and on the go.

This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

Contact Us

News Media Contact:
Rick Aspan, CommScope
+1 708-236-6568 or publicrelations@commscope.com
or
Financial Contact:
Phil Armstrong, CommScope
+1 828-323-4848