GLOBAL LANGUAGE
 
Home > Acerca de nosotros > Noticias > Comunicados de prensa
Comunicados de prensa
SYSTIMAX(R) Solutions Launches Complete 10 Gigabit Ethernet Over Copper Cabling Solution
RICHARDSON, Texas, Dec. 15 /PRNewswire-FirstCall/ -- SYSTIMAX Solutions(TM), the worldwide leader in structured connectivity solutions and services for businesses, today launched a revolutionary cabling solution capable of supporting 10 Gigabit Ethernet. SYSTIMAX Solutions believes it is the first vendor to provide a full UTP solution that fully complies with the latest IEEE 802.3an task force guidelines for 10GBASE-T. SYSTIMAX Solutions has developed the SYSTIMAX(R) GigaSPEED(R) X10D Solution to provide a next generation total solution that supports both the bandwidth needs of today's enterprises and the needs of more demanding applications such as high resolution video, grid computing and Storage Area Network/Network Attached Storage (SAN/NAS).

SYSTIMAX Solutions has a long tradition of producing innovative cabling products that have consistently given enterprise managers the peace of mind that comes with installing a leading edge solution. The GigaSPEED X10D Solution is a natural extension and evolution to existing Category 6/Class E specifications, which SYSTIMAX Solutions was first to launch in 1997 with the GigaSPEED Solution. The GigaSPEED X10D Solution is protected by the industry- leading SYSTIMAX SCS 20-year Extended Product Warranty and Application Assurance.

SYSTIMAX Labs has designed a solution that is compliant with the latest cabling channel requirements set out by the IEEE 802.3an task force. The IEEE 802.3an has adopted new channel specifications for 10GBASE-T known as IEEE Model No.1 PSANEXT (Power Sum Alien Near End Crosstalk) and Insertion Loss. These specifications are also being adopted by the International cabling standard committees in the creation of "new Class E" or "Augmented Category 6" cabling specifications. SYSTIMAX Labs considers these channel specifications technically stable and is introducing an innovative cabling solution that fully supports these requirements over 100 meters including four connections.

Managing the interaction between cables, patch cords and connectors is a major challenge in achieving the performance required to support 10 Gb/s speeds. SYSTIMAX Labs utilized its unique Modal Decomposition Modeling (MDM) tool to evaluate the 1,024 interactions between adjacent, as well as within individual, cabling components to achieve substantial reduction in alien crosstalk (ANEXT or noise from adjacent cables and connectors). In addition, the performance of the GigaSPEED X10D Solution has been tested and qualified in what is viewed as worst-case installation channel test configurations, known as the '6-around-1' cable configuration.

"Through tools such as MDM we believe we are able to provide our customers with cabling that will see them into the future with full channel performance of the system they have installed," said Luc Adriaenssens, Vice President, R&D and Technology, SYSTIMAX Solutions. "With the dramatic rise in the number of end users that are simultaneously activating multiple applications, bandwidth needs are inevitably going to increase. We believe that our GigaSPEED X10D Solution is the most advanced UTP cabling solution offered and are delighted to be the first vendor to provide a full UTP, end-to-end 10 Gigabit solution."

Adriaenssens noted that high-speed technologies such as 10 Gigabit Ethernet are already being deployed in areas of the local area network or LAN. "For the near term," he noted, "these may be concentrated on the interconnection of high-performance servers and switches in data centers, CAD stations and other high performance computing environments, and backbone applications supporting increased use of Gigabit Ethernet to the desktop. However, 10 Gigabit speeds to the desktop are expected to become a reality due to steadily increasing bandwidth demands coupled with reducing cost of interface electronics and the potential adoption of technologies such as grid computing.

"Data centers are expected to be a huge driving force behind the acceptance of 10 Gigabit Ethernet," Adriaenssens continued, "and we expect other institutions, such as banking, medical and movie studios, to be close behind. Businesses that use high-bandwidth applications, multi-site collaboration, streaming media and/or distributed processing technologies are highly likely to be early users of 10 Gigabit Ethernet. Such businesses could certainly benefit from the high-performance capabilities that the GigaSPEED X10D Solution provides."

    The GigaSPEED X10D product portfolio features:
     - GigaSPEED 91 Series Cable, available in plenum, non-plenum and low
       smoke zero halogen versions
     - New, innovative Universal Modular Patch (UMP) Panel
     - MGS500 Outlets
     - GS10E Patch Cords

    About SYSTIMAX Solutions

SYSTIMAX Solutions, a CommScope company, provides integrated end-to-end connectivity solutions for voice, data, video and building management applications in enterprise networks. SYSTIMAX Solutions is a worldwide leader in structured cabling systems, with a product portfolio that includes some of the industry's highest performing copper and fiber solutions.

SYSTIMAX Solutions supplies its high performance and market-leading range of products through a network of highly skilled BusinessPartners. The product range includes the copper based GigaSPEED(R) X10D and GigaSPEED XL Solutions, the fiber-optic LazrSPEED(R) and TeraSPEED(TM) Solutions and the intelligent patching iPatch(R) System. The SYSTIMAX AirSPEED(TM) Solution adds a wireless option to the portfolio. SYSTIMAX Labs and the people who have spearheaded these innovations will continue to play an integral role in the future success of SYSTIMAX Solutions. Currently the company's BusinessPartners install an average of over 1,000 miles (1,600km) of SYSTIMAX cable every day in more than 120 countries worldwide. For further information please visit http://www.systimax.com .

Forward Looking Statements

This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. For a more detailed description of the factors that could cause such a difference, please see CommScope's filings with the Securities and Exchange Commission. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

SOURCE  CommScope, Inc.
    -0-                             12/15/2004
    /CONTACT: Carley Elsdon of SYSTIMAX Solutions, +1-972-792-3445, or
celsdon@systimax.com ; or Michelle Metzger of M-C-C, +1-972-480-8383, or
Michelle_Metzger@mccom.com , for SYSTIMAX Solutions/
    /Web site:  http://www.commscope.com
                http://www.systimax.com /
    (CTV)

CO:  CommScope, Inc.; SYSTIMAX Solutions
ST:  North Carolina, Texas
IN:  CPR NET
SU:  PDT

MH-KM 
-- CLW011 --
7026 12/15/2004 08:00 EST http://www.prnewswire.com
"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995: Statements in this press release regarding CommScope's business which are not historical facts are "forward-looking statements" that involve risks and uncertainties. For a discussion of such risks and uncertainties, which could cause actual results to differ from those contained in the forward-looking statements, see "Risk Factors" in the Company's Annual Report or Form 10-K for the most recently ended fiscal year.
[list]
 
my commscope | eventos | carreras | asistencia tecnica | relaciones con los inversores | derechos y deberes | noticias | sitemap | contactenos