GLOBAL LANGUAGE
 
Home > Про нас > Раздел новостей > Статьи
Статьи
[2009] TIA’s Emerging OM4 Fiber Cabling Standard Sets the Pace for Next-gen Data Center Technology
The wheels are in motion for next-generation data center applications, and the Telecommunications In...
[2009] Performance from Every Angle
Use this downturn to upgrade for the upturn - The current economic climate will increase pressure on...
[2009] It’s Time to Be GREEN: Saving Energy and $$$ in the Data Center
The topic of the day seems to be “Green”, which includes the entire spectrum of using less energy an...
[2008] What should I consider when installing fiber optic cables in my outside plant network?
You must consider four factors when installing FO cables in outdoor environments: tension, radius, s...
[2008] Get Smart Intelligent network infrastructures making strong case
There are several definitions and misconceptions floating around for what makes an intelligent or sm...
[2008] Choosing the EZ-Way: CommScope’s Pre-radiused LC Connectors Decrease Termination Time
With every installation of an optical fiber cable, the ends must be terminated to utilize the cable ...
[2008] Are the mixed-use (MXU) and the multi-dwelling unit (MDU) markets really all they are hyped up to be and why?
These types of installations definitely live up to the expectations and that has made them a common ...
[2008] Parallel Optics Changes the Direction of Network Cabling
Parallel optics technology has been around for some time in high-performance network cabling, but un...
[2008] Rules of Thought for Intelligent Buildings
Building owners and facility managers are encountering on average 15 low-voltage applications on mul...
[2008] Raised Floor vs Overhead Cabling in Data Centers
As part of data center design activities, design professionals are often posed with the question of ...
1 | 2
 
мой commscope | события | достижения | техническая поддержка | отношения с инвесторами | гражданство | новости | карта сайта | связаться с нами