| HICKORY, N.C., April 27 /PRNewswire/ -- CommScope, Inc. (NYSE:
CTV), the leader in high-performance communication cabling,
introduces UltraMedia, the next evolution in Unshielded Twisted
Pair (UTP) cables.
UltraMedia's innovative, round cable design supports
communication speeds greater than 1 Gbps with the industry's
highest attenuation to cross-talk ratio (ACR), which is the best
indicator of how well a network will perform. UltraMedia's 400 MHz
capability, unmatched ACR and precision balance make it the
best-performing UTP cable available. UltraMedia also provides the
greatest usable bandwidth at extended frequencies.
Engineered specifically for high-speed, full-duplex, parallel
transmission protocols that dominate new technologies, UltraMedia
supports voice, video and data applications including 3D imaging
and broadband video.
Twisted pair cables have become one of the most popular ways to
connect intrabuilding networks. Advances in technology have pushed
the limits of standard twisted-pair technology. UltraMedia supports
the intensive demands of multimedia and the next generation of
networks, which must operate at phenomenal speeds.
Superior design and material selection makes this level of
performance possible. UltraMedia is manufactured with
state-of-the-art process controls and comes with a certified test
report attached to every reel of cable.
CommScope is the world's largest manufacturer of coaxial cable
and is a leading supplier of high-performance cables for LAN and
other applications. For more information on more than 6,000
coaxial, fiber and twisted-pair cable products visit CommScope's
web site at www.commscope.com.
SOURCE CommScope, Inc.
CONTACT: Jeff Telling, Market Director-LAN Products, 704-459-5702,
or Phil Armstrong, Director, Investor Relations, 704-323-4848, both
of CommScope, Inc.
Web site: http: //www.commscope.com
|