| HICKORY, N.C., March 23 /PRNewswire/ -- CommScope, Inc. (NYSE:
CTV), a leader in the design and manufacture of high-performance
fiber optic cables, announces it has improved the performance of
its technology award-winning UltraFiber(TM) 62.5 micron fiber
product making it the longest distance/highest bandwidth 62.5
micron fiber on the market today.
UltraFiber, the first fiber product with extended bandwidth, now
offers a new, enhanced bandwidth of 220/1000 MHz-km and laser
certification. These features allow it to support the IEEE 802.3z
Gigabit Ethernet standard to distances of 500 meters at the 850
nanometer (nm) wavelength and 1200 meters at the 1300 nm
wavelength. This distance performance more than doubles the
industry standard of 220 meters and 500 meters at the two
respective wavelengths. In addition, UltraFiber is laser-certified
for use with both vertical cavity surface emitting lasers (VCSELs)
and standard single mode lasers and will not require the use of
offset patch cords for proper operation.
"Many users of standard fiber products will find they have
distance limitations when they attempt to migrate from low speed to
high speed applications, potentially forcing them to undergo costly
re-cabling," stated Teresa Munsey, CommScope's Fiber Optic Product
Manager for Local Area Networks. "UltraFiber gives our customers
the ability to support low speed 10 megabit per second light
emitting diode (LED) applications all the way up through 1 gigabit
per second laser applications in one fiber product. UltraFiber is
currently the only 62.5 micron fiber that has the bandwidth or
laser certification needed to support Gigabit Ethernet out past
1,000 meters."
CommScope's UltraFiber is part of a complete fiber optic product
offering which includes outside plant loose tube cables,
self-supporting loose tube cables, riser-rated indoor/outdoor loose
tube cables, riser-rated indoor/outdoor tight buffer cables, indoor
premise cables and a variety of specialty cables. CommScope is the
world's largest manufacturer of coaxial cable and a leading
supplier of high-performance fiber optic and twisted pair cables
for telecommunications applications.
Statements in this press release which are other than historical
facts are intended to be "Forward Looking Statements" within the
meaning of the Securities Exchange Act of 1934, the Private
Securities Litigation Reform Act of 1995 and other related laws.
The cautionary statements contained in Exhibit 99 to CommScope's
Form 10-Q for the quarter ended September 30, 1999 are incorporated
herein by reference.
Visit CommScope at www.commscope.com
SOURCE CommScope, Inc.
Web site: http: //www.commscope.com
CONTACT: Teresa Munsey, Fiber Optic Product Manager for LAN,
828-459-5251, or e-mail, tmunsey@commscope.com , or Betsy Lambert,
APR, Media Relations, 828-323-4873, or e-mail,
blambert@commscope.com , both of CommScope, Inc.
|