Wireless technology has become the primary communications method in public venues and commercial buildings for both personal communication and first responder services. As wireless penetration rates approach and exceed 100%, users demand that their wireless connected electronic devices work just as effectively indoors as they do outdoors. First responders require reliable, ubiquitous radio coverage to ensure the safety of the public as well as themselves in emergency situations. CommScope's In-Building Wireless (IBW) Solution provides the products and services to address the most complex mobile challenges.
Experience and Excellence Make CommScope’s In-Building Wireless Solutions the Right Choice
In a world transformed by communications, convergence of voice, data and video brings today's mobile society together and enhances our lives, workplaces and communities. CommScope’s In-Building Wireless Solutions can help shape the mobile future. With a comprehensive product portfolio, CommScope supports today’s mobile society and helps build the foundation for reliable wireless service. CommScope has world-leading wireless operator customers, while through its enterprise division does business with building owners and tenants the world over. This customer base and corresponding product portfolio makes CommScope unique in supporting all communication needs to the sector. CommScope provides a one-stop source for managing the entire lifecycle of a wireless network. The IBW product line offers a complete solution that serve 2G, 3G, and 4G wireless networks.
CommScope is a recognized world leader in infrastructure solutions for communications networks, and its In-Building Wireless (IBW) product line is an integral piece to CommScope’s network infrastructure solution. CommScope enables customers around the world to create a connected environment that supports current and future business and technology opportunities by providing the right network infrastructure solution.
Employees and guests; suppliers and customers all have come to expect reliable connectivity wherever they may be, from their car to the office. The promise of mobility is here and CommScope's IBW Solutions ensure that it has no boundaries.
CommScope's Wired for Wireless Solution is a cost effective solution designed to allow Enterprise customers to prepare their buildings for wireless coverage. By deploying broadband coaxial cable and antennas throughout a building during the construction phase, custom design is eliminated and system costs are lower. The solution paves a path for the in building wireless needs of today and tomorrow. CommScopes Wired for Wireless Solution includes coaxial cables, connectors, antennas and cable management apparatus, connected together in such a way as to provide ubiquitous wireless coverage through the entire structure. Unique Wired for Wireless guidelines for antenna placement eliminate the need for costly and time consuming RF site surveys and protects the wireless performance inside the building from the future changes of the outdoor network. CommScopes future-proof and cost-effective platform for uniform coverage will meet the ever increasing indoor wireless requirements. CommScopes Wired for Wireless Solution has the Enterprise Covered.
High performance indoor antennas, coaxial cables, connectors, and cable management apparatus ensure that the Wired for Wireless Solution delivers a cost and performance optimized platform that is ready for carrier-neutral and uniform wireless coverage in Enterprise buildings.
Indoor Antennas
Cell-Max™ Omnidirectional Antenna The CELLMAX-O-CPUSE antenna is a ceiling mounted omnidirectional indoor antenna designed for the 698-960 MHz and 1710-2700 MHz frequency ranges. It supports all modulation formats and technology including, Analog, iDEN, GSM, GPRS, EDGE, UMTS, HSDPA, HSUPA, LTE, CDMA2000, EV-DO, Wi-Fi, Wi-Max and many more.
Cell-Max™ Directional Antenna The CELLMAX-D-CPUSE antenna is a wall mounted directional indoor antenna designed for the 698-960 MHz and 1710-2700 MHz frequency ranges. It supports all modulation formats and technology including, Analog, iDEN, GSM, GPRS, EDGE, UMTS, HSDPA, HSUPA, LTE, CDMA2000, EV-DO, Wi-Fi, and Wi-Max and many more.
Cables and Connectors
FXL-540-NHR HELIAX® cable The FXL-540-NHR cable is a flexible inch 50 ohm coaxial cable, with a black PE jacket, a smoothwall aluminum outer conductor, foam PE dielectric and a copper clad aluminum inner conductor. With its light-weight and cost effective construction, the FXL-540-NHR cable is easy to install and delivers excellent transmission performance.
EZFit® Connector for FXL-540-NHR cable The 540EZNMV2 EZFit connector is a high performance N-type male connector that is a perfect match for the FXL-540-NHR cable. The 540EZNMV2 is a small and lightweight two piece connector designed for easy installation and optimal electrical performance. High precision cable preparation and 540EZNMV2 connector attachment is achieved with the 12-HPT EZFit hand prep tool or the 540-ZPT EZFit drill prep tool.
AL4RPV-50 HELIAX® cable The AL4RPV-50 cable is a flexible inch 50 ohm plenum rated coaxial cable, with an off-white PVC jacket, a corrugated aluminum outer conductor, a PE Spline air dielectric and a copper clad alumimum inner conductor. With its light-weight and cost effective construction, AL4RPV-50 cable is easy to install and delivers excellent transmission performance.
Positive Stop™ Connector for AL4RPV-50 cable The L4TNM-PSA Positive Stop connector is a high performance N-Type male connector that is the perfect match for the ALPRV-50 cable. The L4TNM-PSA Positive Stop connector is a small and lightweight connector designed for ease of installation and optimal electrical performance. The L4TNM-PSA connector can be installed with standard tools. Cable preparation for L4TNM-PSA connector attachment can be achieved with MCPT-L4 EASIAX manual cable prep tool or the drill-assisted EASIAX Plus CPT-L4ARC1 automated cable prep tool.
Organizers
Wired for Wireless® Wall Organizer The Wired for Wireless Wall Organizer is designed to secure the terminated FXL-540-NHR or AL4RPV-50 inch coaxial cables in a telecommunications room wall, and provides mounting positions for the 2-way and/or 4-way splitters that will be required to split the active equipment signal to the various antennas. A single Wall Organizer can secure up to eight terminated FXL-540-NHR or AL4RPV-50 coaxial cables. Additional Wall Organizers may be installed side by side to secure up to eight additional cables per organizer.