Home > Acerca de nosotros > Noticias
Noticias
[April 27, 1998]
CommScope Introduces UltraMedia(TM), The Extended-Bandwidth UTP Cable That Defines A New Standard In LAN Performance
HICKORY, N.C., April 27 /PRNewswire/ -- CommScope, Inc. (NYSE: CTV), the leader in high-performance communication cabling, introduces UltraMedia, the next evolution in Unshielded Twisted Pair (UTP) cables.

UltraMedia's innovative, round cable design supports communication speeds greater than 1 Gbps with the industry's highest attenuation to cross-talk ratio (ACR), which is the best indicator of how well a network will perform. UltraMedia's 400 MHz capability, unmatched ACR and precision balance make it the best-performing UTP cable available. UltraMedia also provides the greatest usable bandwidth at extended frequencies.

Engineered specifically for high-speed, full-duplex, parallel transmission protocols that dominate new technologies, UltraMedia supports voice, video and data applications including 3D imaging and broadband video.

Twisted pair cables have become one of the most popular ways to connect intrabuilding networks. Advances in technology have pushed the limits of standard twisted-pair technology. UltraMedia supports the intensive demands of multimedia and the next generation of networks, which must operate at phenomenal speeds.

Superior design and material selection makes this level of performance possible. UltraMedia is manufactured with state-of-the-art process controls and comes with a certified test report attached to every reel of cable.

CommScope is the world's largest manufacturer of coaxial cable and is a leading supplier of high-performance cables for LAN and other applications. For more information on more than 6,000 coaxial, fiber and twisted-pair cable products visit CommScope's web site at www.commscope.com.
SOURCE CommScope, Inc.
CONTACT: Jeff Telling, Market Director-LAN Products, 704-459-5702, or Phil Armstrong, Director, Investor Relations, 704-323-4848, both of CommScope, Inc.
Web site: http: //www.commscope.com

"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995: Statements in this press release regarding CommScope's business which are not historical facts are "forward-looking statements" that involve risks and uncertainties. For a discussion of such risks and uncertainties, which could cause actual results to differ from those contained in the forward-looking statements, see "Risk Factors" in the Company's Annual Report or Form 10-K for the most recently ended fiscal year.
[list]

 
my commscope | eventos | carreras | asistencia tecnica | relaciones con los inversores | derechos y deberes | noticias | sitemap | contactenos