Wiring up a fiber/power junction box on a cell tower is like the game Operation, only there isn’t a buzzer that goes off when you’ve made a mistake. Instead, the remote radio units won’t work right or performance will be degraded in some manner. In today’s blog post, Chris Stockman introduces CommScope’s latest solution, HELIAX FiberFeed Direct, for making fiber connections a more simple operation.
That’s what makes me think of the game Operation. Only there is no buzzer that goes off when you don’t wire the junction box correctly. Instead, the RRUs won’t work right, or performance is degraded for subscribers, and you likely need to climb back up to fix the problem, costing more time and money. The ramifications are a little greater in real-life than in a board game.
The complexity of wiring junction boxes is part of the reason why CommScope is offering a new alternative to them—the breakout canister. Part of the new HELIAX FiberFeed Direct solution, the breakout canister comes pre-wired on the end of the hybrid trunk cable. The power and fiber tails can easily be plugged right into the RRUs, foregoing the need to wire up a junction box. The intended result is much easier installations with more reliable results.
HELIAX FiberFeed Direct will mate to any RRU model, reducing the number of overall connections and cutting fiber installation time by half. CommScope believes its FiberFeed Direct customers will also realize about a third less tower loading due to the canister’s physical size.
In the meantime, are there any questions about FiberFeed Direct that I can answer?