Tower_360X203The Top Fiber Questions blog series is dedicated to answering the most frequently asked questions in the industry. From now until the end of the year, we hope to provide great answers. Most importantly, we’d love for you to ask your fiber questions in the comments section below. 

Question:

Will fiber be the best solution to connect cellular network radios in the future? 

Answer:

That is the consensus. Mobile network operators will opt for fiber as the preferred technology for backhaul and fronthaul to cellular network radios wherever possible because of the ever-increasing bandwidth requirements of today and into the future.

CLICK TO TWEET: Is fiber the future of radio towers? Read more from CommScope's Wes Oxlee.

Fiber offers the network operators many benefits such as:

  • Capacity—Fiber can keep pace with growing backhaul requirements without the throughput and distance limitations of other technologies.
    • Scalability—Capacity can be easily expanded through multiplexing wavelengths on existing strands or by pulling new strands through existing conduit.
    • Reliability—Fiber offers superior backhaul uptime, leading to increased subscriber satisfaction.   
    • Redundancy—Fiber can provide critical microcell backup for the continuing flow of network traffic if the primary backhaul link fails.  

    The density of radios for future cellular will drive the requirement for network convergence between wired and wireless traffic, increasing the requirement for fiber network solutions that focus on providing the density, accessibility and flexibility to support multiple applications needed for the future.

    Another major driver is to reduce power usage and optimize space utilization at the tower. Many operators are now transitioning to C-RAN (centralized RAN) architecture—and fiber is key to the transition. With C-RAN, baseband units (BBUs) are moved away from the bottom of the tower and into central offices or BBU pooling locations, which can be located many kilometers away.

    At the central office, the BBUs from multiple cell sites are pooled and connected to the remote radio head via fronthaul connectivity (to carry data from the cell sites to the BBU pool) and backhaul (to carry data from the BBUs back to the core network).

    C-RAN offers an effective way to increase the capacity, reliability and flexibility of the network while lowering operational costs. It is also a necessary step along the path to cloud-RAN, where the BBU functionality will become “virtualized”—allowing for great elasticity and scalability for future network requirements.

    About the Author

    Wes Oxlee

    Wes Oxlee is Director Wireless Connectivity Solutions at CommScope Connectivity Solutions business unit of CommScope. Wes has 32 years of telecommunications industry experience with a primary focus on optical fibre external plant networks. Following a 16 year career with Telstra and NDC, where he was the National Technical Specialist for Fibre Optics External Plant, he joined CommScope in 2000. Wes is a Certified Fibre To The Home professional and has been an integral part of CommScope’s team in NBN, Reliance & UFB as well as a wide number of FTTH projects throughout the world. In his current role Wes is responsible for formulating innovative connectivity solutions for wireless networks.

    See all posts by this author

    Add Your Comment

    Please submit your comment using the form below

     
    (required)