SUNNYVALE, CA — March 5, 2013 – Ruckus Wireless, Inc. (NYSE: RKUS) today announced the launch of its dual-band concurrent ZoneFlex™ 7055 Wi-Fi wall switch, the first of its kind in the world. The ZoneFlex 7055 Wi-Fi wall switch gives hotel and resort operators an elegant, low-cost and inconspicuous solution that leverages their existing wired infrastructure, while enabling the delivery of high-speed Wi-Fi to support an ever-expanding assortment of IP-based guest services over multiple virtual LANs (VLANs).
The only integrated solution in the industry to offer the simultaneous operation of 2.4 and 5 GHz 802.11n Wi-Fi along with wireless meshing, the ZoneFlex 7055 Wi-Fi wall switch uniquely combines wired and wireless connectivity within a universal low-profile form factor (13.6 cm square by 30 cm deep) that fits into any standard United States or European electrical junction box, among others.
Since introducing the first 802.11n Wi-Fi wall switch in 2009, Ruckus Wi-Fi wall switches have now been installed in over 100,000 hotel rooms in some of the world’s most prestigious properties such as the Mandarin Oriental New York, the Atlantis Paradise Island Resort in the Bahamas, the Borgata Hotel Casino and Spa in Atlantic City, the Star City Casino in Sydney, the Ritz-Carlton Bahrain Hotel and Spa, and many more.
“The ZoneFlex 7055 now lets us better support new smartphones and future 802.11ac devices that only operate within the channel-rich 5 Gigahertz band,” said David Heckaman, VP of Information Technology for Mandarin Oriental in North America. “Like many hotels, the costs of running additional Ethernet cabling into every room to enable new services like IPTV while needing to provide a reliable Wi-Fi experience we’re daunting. This new Ruckus Wi-Fi wall switch will effectively solve these problems for us.”
One of the world’s most prestigious hotels, the five-star Mandarin Oriental New York, situated in New York’s Columbus Circle overlooking Central Park, is one of the first organizations to test the new ZoneFlex 7055 Wi-Fi wall switch and has been using ZoneFlex 7025 Wi-Fi wall switches in hundreds of its guest rooms.
“Since installing Ruckus Wi-Fi wall switches, we’ve seen phenomenal improvements in performance and reliability,” said Heckaman. “But the ultimate endorsement has been the resounding silence we’ve heard from our guests. Wi-Fi complaints are now the exception and not the rule.” Mandarin Oriental New York is one of seven acclaimed Mandarin Oriental hotels that have now installed Ruckus Smart Wi-Fi, including their properties in Tokyo, Manila, Jakarta, Sanya (China), London, and Hong Kong.
Introducing the ZoneFlex 7055
Functioning as a standalone device or managed centrally by the Ruckus ZoneDirector™ wireless LAN (WLAN) controller, the ZoneFlex 7055 Wi-Fi wall switch is an ideal solution for hotels, schools and large institutional organizations wishing to address the proliferation of 5 GHz capable client devices like the Apple iPhone 5 and others, while continuing to support 2.4 GHz and wired access.
Featuring dual 802.11n (2x2:2) radios and 16 virtual WLANs (SSIDs), the ZoneFlex 7055 Wi-Fi wall switch offers up to 600 Mbps of throughput. The ZoneFlex 7055 also features a Gigabit Ethernet uplink port, plus four front-facing Fast Ethernet ports that provide wired connectivity for guests, IPTV systems, and other networked in-room devices such as printers, minibars and environmental control systems.
The new Ruckus ZoneFlex 7055 delivers 802.3af Power-over-Ethernet (PoE) to power devices such as a Voice over Internet Protocol (VoIP) phone, using one of its front-facing Ethernet ports. An additional pass-through port allows direct wired connectivity for devices that need to bypass the Ethernet switch altogether or provide a guest with VLAN connectivity. It can be powered by 802.3af/PoE through the uplink port, which means only a single cable drop is required behind the wall. In the absence of PoE, a standard power adapter can also power the ZoneFlex 7055.
With support for Ruckus Wireless SmartMesh Networking, the ZoneFlex 7055 is an excellent solution for buildings where running Ethernet cable behind the walls is difficult or prohibitively expensive. In-room wired and wireless access can be provided in several rooms, each hosting a single ZoneFlex 7055 powered by a power adapter and meshed with a centrally wired (root) access point (AP). Since only the root AP requires a cabled Ethernet uplink, multiple rooms are covered with just a single cable drop.
Pricing and Availability
Shipping now, the new Ruckus ZoneFlex 7055 Wi-Fi wall switch has an MSRP of $369 (USD), and is available through authorized Ruckus Big Dog resellers worldwide.
ABOUT RUCKUS WIRELESS
Headquartered in Sunnyvale, CA, Ruckus Wireless (NYSE: RKUS) is a global supplier of advanced wireless systems for the rapidly expanding mobile Internet infrastructure market. With 2012 revenues of $214.7 million, the company offers a wide range of indoor and outdoor "Smart Wi-Fi" products to mobile carriers, broadband service providers, and corporate enterprises, and has more than 21,700 end-customers worldwide. Ruckus technology addresses Wi-Fi capacity and coverage challenges caused by the ever-increasing amount of traffic on wireless networks due to accelerated adoption of mobile devices such as smartphones and tablets. Ruckus invented and has patented state-of-the-art wireless voice, video, and data technology innovations, such as adaptive antenna arrays that extend signal range, increase client data rates, and avoid interference, ensuring consistent and reliable distribution of delay-sensitive multimedia content and services over standard 802.11 Wi-Fi. For more information, visit https://www.ruckuswireless.com.
Ruckus, Ruckus Wireless, ZoneDirector, and ZoneFlex are trademarks of Ruckus Wireless, Inc. in the United States and other countries. All other product or company names may be trademarks of their respective owners.