From AI to the Edge: Why Fiber Networks Matter More Than Ever

Technology continues to evolve at a rapid pace, putting increasing pressure on network infrastructure to deliver higher bandwidth, lower latency and more reliable connectivity. The recent breakthroughs in Artificial Intelligence (AI) have accelerated this trend even further, sparking a global race to develop the most powerful models.

Training these AI models is extremely compute intensive. It relies on massive, repeated matrix operations that require significant processing power. Most of this activity takes place inside data centers, which has increased the demand for new facilities and higher-capacity infrastructure.

What comes next?

As AI models continue to improve, they are enabling a wide range of new applications. Today, the most visible example is Large Language Models (LLMs), which can generate, summarize and predict human-like text and code, but they are just one of many use cases. There are countless applications still emerging.

What’s important is how these applications are delivered. Once a model is trained, it is deployed for inference, the prediction phase. Unlike training, inference doesn’t stay confined to the data center. It becomes an interaction between users and the systems hosting the model.

Those users could be anywhere, at home, in the office, in a car or outdoors. This shift creates a new requirement: delivering high-bandwidth, low-latency all the way to the end user, wherever they are.

Why fiber optics?

Fiber optics offer a clear advantage in meeting these demands. They offer unmatched symmetrical speeds, ultra-low latency and high reliability. Perhaps most importantly, fiber has virtually unlimited bandwidth potential—capacity can be increased by upgrading the electronics at each end without replacing the underlying infrastructure.

For these reasons, fiber is the technology of choice for connecting data centers, central offices and extending networks all the way to the edge. But the real opportunity, and challenge, is extending fiber deeper into communities through Fiber to the Home (FTTH).

Is FTTH deployment too expensive?

Not necessarily. With proper planning, FTTH can be both cost-effective and scalable. Service providers face several challenges, including deployment speed, availability of skilled installers and overall cost. Broadband network architecture plays a major role in addressing these challenges.

In many markets, the first provider to deploy fiber captures the highest share of customers. That makes speed and coverage critical. Providers are not just trying to reduce costs; they 
are trying to maximize coverage within limited budgets and timelines.

Passive Optical Network (PON) technology has been a key enabler of FTTH by reducing both equipment and fiber costs, particularly on the feeder side of the network. It also introduces flexibility in how networks are designed, especially in how and where optical splitting occurs.

Historically, centralized splitting was the preferred approach. This was largely due to dense urban deployments and the economics of central office equipment, where maximizing OLT port utilization made sense; however, the landscape is changing.

As deployments move into lower-density and rural areas—and as central office equipment becomes more accessible and cost-effective—centralized architectures are not always the best option. In these scenarios, centralized designs require longer distribution fiber runs (F2), which increases cost.

Distributed and cascaded architectures offer an alternative by moving splitters closer to the end user. This reduces distribution fiber length and can significantly lower overall costs, including materials, connectivity and civil infrastructure such as conduit and aerial construction.

Choosing the right network architecture

There is no one-size-fits-all solution; the optimal FTTH architecture depends on factors such as network environment (rural, suburban, or urban), required flexibility, scalability, and deployment cost considerations. The following outlines the most common topologies for comparison:

Each approach has its advantages. As deployments expand into less dense areas, architectures like daisy chain and optical tap often become more attractive. They enable faster rollout and more efficient use of resources, allowing providers to cover larger geographic areas with the same budget and timeframe.

Building for the future

Whether the network is centralized, distributed or cascaded, CommScope provides a comprehensive portfolio of fiber cable and connectivity solutions to support reliable, future-ready networks.

CommScope splice closures, powered by FOSC® sealing technology, are designed for both flexibility and durability. They simplify fiber splicing while also supporting efficient customer connections. These sealed closure systems are built to perform in demanding environments and support long-term network reliability.

© 2026 CommScope Technologies LLC, an Amphenol company.  All rights reserved.  CommScope and the CommScope logo are registered trademarks of CommScope and/or its affiliates in the U.S. and other countries.  For additional trademark information see https://www.commscope.com/trademarks. All product names, trademarks and registered trademarks are property of their respective owners.