Aurora Networks™ (ANS) and RUCKUS® Networks are now Vistance™ Networks
Visit their new site for all products and content
Aurora Networks™ (ANS) and RUCKUS® Networks are now Vistance™ Networks
Visit their new site for all products and content
Andrew, the CommScope, Inc. division that is a global leader in wireless communication systems and products, is going indoors with its Invex.NxG™ wireless drive-test system, offering new equipment that makes designing and testing indoor wireless coverage systems easier.
The i.Send™ portable transmitter imitates wireless base station signals by broadcasting radio frequency (RF) signals that allow for coverage measurements indoors. Network designers can use the i.Send transmitter to verify optimal antenna positioning for indoor distributed antenna systems (DAS) and as a low power source for testing the design and functionality of RF repeaters and base stations.
“The i.Send transmitter is a unique tool for verifying in-building coverage, DAS and repeater system design,” said John Baker, vice president and general manager, Network Solutions, Andrew. “Such a device should help operator engineers maximize the performance of their indoor networks prior to final installation.”
The portable Invex.NxG i.Send offers over 20 dBm of transmit power for up to four hours between battery charges and supports GSM, CDMA, UMTS and W-CDMA frequency bands with user-settable channel and message parameters. Users can configure i.Send via a Wi-Fi connection, selecting the desired frequency and modulation schemes, with the ability to set the parameters within the scheme. For ease of operation, the unit is placed in transmit or standby mode via the Wi-Fi connection.
Andrew’s Invex.NxG wireless drive-test system enables wireless operators to view their own and their competitors’ wireless voice and data services from the perspective of the subscriber by providing critical quality-of-service (QoS) measurements. Invex.NxG identifies failed originations, abnormal ends, call setup time, and call quality for improving voice service levels. It also performs packet data testing for analyzing upload/download throughput speeds for data services and can be used by field personnel for independently checking network signal strength and identifying base station locations and sectors, assisting them in their jobs.
Invex.NxG and i.Send are trademarks of CommScope, Inc.
About CommScope
CommScope, Inc. (NYSE: CTV)(www.commscope.com) is a world leader in infrastructure solutions for communication networks. Through its Andrew® brand, it is a global leader in radio frequency subsystem solutions for wireless networks. Through its SYSTIMAX® and Uniprise® brands, CommScope is a world leader in network infrastructure solutions, delivering a complete end-to-end physical layer solution, including cables and connectivity, enclosures, intelligent software and network design services, for business enterprise applications. CommScope also is the premier manufacturer of coaxial cable for broadband cable television networks and one of the leading North American providers of environmentally secure cabinets for DSL and FTTN applications. Backed by strong research and development, CommScope combines technical expertise and proprietary technology with global manufacturing capability to provide customers with infrastructure solutions for evolving global communications networks in more than 130 countries around the world.
This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. For a more detailed description of the factors that could cause such a difference, please see CommScope’s filings with the Securities and Exchange Commission. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
CommScope
News Media Contact:
Bill Walter
+1 708-236-6593 or publicrelations@andrew.com
or
CommScope
Investor Contact:
Phil Armstrong
+1 828-323-4848