Aurora Networks™ (ANS) and RUCKUS® Networks are now Vistance™ Networks
Visit their new site for all products and content
Aurora Networks™ (ANS) and RUCKUS® Networks are now Vistance™ Networks
Visit their new site for all products and content
CommScope, Inc. (NYSE: CTV), the world leader in the design and manufacture of cable and connectivity solutions for communications networks, working together with theDefense Information Systems Agency (DISA) Joint Interoperability Test Command (JITC), has received an Interoperability Assessment and a Standards Conformance certification for the SYSTIMAX iPatch Real-time Infrastructure Management System. The ability to manage, configure and monitor the physical interconnections between network elements can be a challenge to any organization, particularly one with a network as complex as the U.S. Department of Defense (DoD). In its February 2007 report, the JITC analysis determined that the SYSTIMAX iPatch System meets the current DoD and industry standards; provides network physical layer management within the complex DoD network architecture in a secure and reliable manner. The DoD believes its analysis represents a thorough demonstration of a product's ability to provide protocol compliance, stability, scalability, management and security to DoD networks.
"CommScope is proud to be able to support the DoD and the people who depend on the network," said Mark Peterson, senior vice president, global marketing, enterprise, CommScope. "We're obviously very pleased that our iPatch Solution performed so well. We believe this real-time infrastructure management system provides a significant new capability to the defense community and will enhance the DoD's ability to manage its communications network. We look forward to continuing our work with the US Government and the DoD."
The test effort consisted of three phases. The standards conformance phase tested the iPatch System in an isolated environment using test equipment to transmit and receive traffic flows through the isolated system. In the next phase, the system was integrated into a representative DoD network and test equipment was used to transmit and receive traffic across the network. The equipment was then used to measure the number of data frames received and the packet delay time. The measurements revealed no packet loss, 100 percent throughput and less than 10 microseconds latency for all packet sizes at all interface speeds. The final phase of testing captured and analyzed data transmissions between the SYSTIMAX iPatch Rack Manager Plus and SYSTIMAX iPatch System Manager Personal Computer and did not find any iPatch System vulnerabilities that external (or internal) hackers could exploit.
When deployed, the SYSTIMAX iPatch System will provide the DoD with an integrated, real-time infrastructure management solution comprising intelligent copper and fiber patch panels, a Rack Manager Plus unit (for managing and monitoring the panels in a rack or cabinet) and System Manager Software. These combined elements simplify the management and control of the physical interconnections between elements of the communications network. The system will also manage patching (moves, adds and changes), provide physical layer tracing and assist in optimized port utilization. Most importantly, the iPatch System performs Simple Network Management Protocol auto-discovery of network elements and generates alarms whenever unexpected or unauthorized interconnections occur in the network - ensuring that corrective actions are taken quickly.
About SYSTIMAX Solutions
SYSTIMAX Solutions from CommScope (NYSE: CTV) is a worldwide leader in structured cabling systems and provides integrated end-to-end connectivity solutions for video, voice, data and building management applications in both wired and wireless enterprise networks.
SYSTIMAX Solutions supplies its high-performance and market-leading range of products through a network of highly skilled BusinessPartners. The product range includes the copper-based GigaSPEED X10D and GigaSPEED XL Solutions, the fiber optic LazrSPEED(R) and TeraSPEED(TM) Solutions and the iPatch(R) Real-time Infrastructure Management System. The SYSTIMAX AirSPEED(TM) Solution adds a wireless option to the portfolio. Drawing on their Bell Labs heritage, the people of SYSTIMAX Labs who have spearheaded these innovations will continue to play an integral role in the future success of SYSTIMAX Solutions. Currently the company's BusinessPartners install an average of over 1,000 miles (1,600km) of SYSTIMAX cable every day in approximately 130 countries worldwide.
For further information please visit http://www.systimax.com
Forward-Looking Statements
All statements in this press release that are not historical facts should be considered forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. For a more detailed description of the factors that could cause such a difference, please see CommScope's filings with the Securities and Exchange Commission. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
for SYSTIMAX Solutions
Sadie McCrary of M-C-C, +1-972-480-8383 x 222
Sadie_McCrary@mccom.com
or
Fiona Nolan of CommScope, +011-353-1-204-2000
fnolan@systimax.com
Web site: http://www.commscope.com
http://www.systimax.com /(CTV)