CommScope Launches the Rapid Fiber Connect™ Platform at NVIDIA GTC 2026

CommScope brought some exceptionally big news to the show. We introduced our new, globally-available Rapid Fiber Connect platform to the world.

 

The NVIDIA GTC AI Conference and Expo in San Jose, CA ran from March 16 – 19, and this year, CommScope brought some exceptionally big news to the show. We introduced our new, globally-available Rapid Fiber Connect platform to the world, and for super-high density AI data centers, it is truly a game-changer.

 

Simply put, the Rapid Fiber Connect platform is a system of three components designed to work in harmony to accelerate time-to-service, streamline scale-out deployments and reduce the amount of labor and floor disruption involved in rolling in new racks.

Panels and cables, simplicity and speed

The platform consists of GPU panels, switch panels and trunk cables with Mass Insert connectors to connect the panels. Together, they make it easier for AI data center operators to configure new racks offsite—or at least off the floor—and roll them in, ready to connect and turn up. Each part of the platform is designed to flex to accommodate growing network demand and evolving architectures, such as NVIDIA’s NVL72 72-GPU rack-system infrastructure.

  • Rapid Fiber Connect GPU panels feature front-access only designs that accommodate up to 960 fibers, making it a smart choice for high-density racks with power/cooling connections blocking off rear access
  • Rapid Fiber Connect switch panels provide front and rear access designs capable of supporting up to 1,728 fibers each. They’re stackable to support the high fiber counts required for the switch cabinets in AI data center GPU network.
  • Trunk cables with Mass Insert connectors are available in singlemode and multimode options to connect between racks and across pods, in a range of lengths and fiber counts to accommodate different applications.

As the AI data center race heats up, the Rapid Fiber Connect platform can help speed up deployments that would otherwise be hampered by labor shortages or network complexity obstacles. They’re ready to roll out now, so you can start rolling in racks faster. You can learn all about the solution here!

The shuffle story

While at the show, I also found a great deal of interest in AI data center GPU network architecture and multi-plane networks. Multi-plane networks allow you to break the individual lanes from each GPU out into separate planes, producing multi-path options for data transmit/receive and increasing the total possible GPU count, all with only two tiers of switching. This multi-plane network is achieved by applying a shuffle into the network architecture at the first layer of switching.

CommScope offers the products you may need for efficiently integrating the shuffle into the network. While there are multiple ways to implement shuffle, my best recommendation is as follows:

  • GPU Cabinet: Rapid Fiber Connect panel, pre-integrated offsite with GPU connections
  • Bundled array: Mass Insert MMC connecting to the Rapid Fiber Connect panel in GPU cabinet, and individual MPO12/8 breakouts on switch cabinet end
  • Switch cabinet: Propel® Shuffle modules applying the shuffle, with patchcords then connecting down to the switches

Get the guideand get the latest!

One thing that I (and likely other GTC 2026 attendees) took away from the show is that AI data centers are evolving fast. CommScope® innovation is working hard to keep our customers ahead of the curve, and all that innovation is on display than our brand-new ordering guide for NVIDIA GB200/GB300 NVL72 AI architectures. It features our most cutting-edge technologies, including the new Rapid Fiber Connect platform, built to turn complexity into clarity for the highest-density AI data centers.

Of course, new GPU and switching platforms are entering the market all the time, and that’s why I—and everyone at CommScope—is committed to working at the forefront of evolving technologies. We collaborate closely with our customers so we can better understand their unique network requirements. Every application is different, and our approach is built on breaking down complex architectures, understanding real‑world deployment needs, and delivering smarter solutions that are optimized for performance, scalability and reliability.

Energized by the excitement of GTC 2026, CommScope is excited to support your next‑generation AI deployments with proven expertise and innovative solutions—and our new Rapid Fiber Connect platform is just the latest example of how our commitment translates into real innovation.

 

© 2026 CommScope Technologies LLC, an Amphenol company.  All rights reserved.  CommScope and the CommScope logo are registered trademarks of CommScope and/or its affiliates in the U.S. and other countries.  For additional trademark information see https://www.commscope.com/trademarks. All product names, trademarks and registered trademarks are property of their respective owners.