Aurora Networks® (ANS) and RUCKUS® Networks are now Vistance Networks
Andrew Corporation, a global leader in communications equipment and systems, has introduced two new earth station antenna (ESA) products designed to provide world class Andrew quality at prices competitive with less capable units available elsewhere.
The two new lines, the Andrew 4 Meter Class High Value ESA and the pre-engineered Andrew Earth Station Terminals (EST), meet the cost of ownership needs of customers and systems integrators worldwide. They will be introduced this week at the Satellite 2007 show in Washington, D.C.
“The cost of purchasing an antenna and related system are only part of its ownership cost,” said Russell Dearnley, director, Earth Station Antennas and Systems, Satellite Communications, Andrew Corporation. “That initial savings can be quickly consumed by higher costs for shipping, installation, and support of less reliable systems. These new Andrew products are designed to provide a lower cost of ownership, while leveraging Andrew’s wealth of experience in serving the needs of specific industries and world regions.”
The new products are well suited for the needs of customers and systems integrators operating in various industries.
4 Meter Class High Value ESA
The Andrew 4 Meter Class High Value ESA is well suited for emerging markets, such as Africa, Latin America, and Asia, which require robust systems with a low cost of ownership. The new 4 meter class antenna will replace Andrew’s existing low cost 3.7 meter product with a view of total cost of ownership, augmenting Andrew’s premier 4 meter class antenna offering and Andrew’s full line of ESA offerings in use to transmit signals to and from satellites for broadcast, cellular backhaul, and general satellite applications.
The unit offers advantages that provide lower cost and ease of use for Andrew customers around the world. For example, it can be installed without a crane, and moved inside buildings via regular elevators and stairwells. In addition, transport costs are lower because Andrew can load up to six units per 20 foot container.
Earth Station Terminals
Andrew is bringing to market several new pre-engineered Earth Station Terminals that provide major savings by eliminating the need for custom design. They provide cost-effective one- and two-way satellite communications for specialized customer segments. Andrew anticipates strong demand for these units in cellular backhaul, and single carrier per channel applications for public and private broadcast networks. The pre-engineered Earth Station Terminals are a teaming of Andrew’s 4 meter and 5 meter class antennas, with a number of standardized electronic packages to provide a quick-to-deploy solution for various bandwidth requirements.
Andrew’s Satellite Communications Group, part of the Antenna and Cable Products Segment, provides a complete line of antennas from 46 centimeters to 11.5 meters for all enterprise, government/military, and consumer satellite communications applications. Andrew-designed and -built products—which cover C, Ku, K, X, and the emerging Ka band—include approved earth station antenna hubs and gateways for broadband and broadcast, VSAT broadband antennas for consumer and enterprise customers, DBS antennas for home satellite broadcast systems, and complete installation and testing services.
About Andrew Corporation
Andrew Corporation (NASDAQ: ANDW) designs manufactures, and delivers innovative and essential equipment and solutions for the global communications infrastructure market. The company serves operators and equipment manufacturers from facilities in 35 countries. Andrew (www.andrew.com), headquartered in Westchester, IL, is an S&P MidCap 400 company founded in 1937.
Forward Looking Statements
Some of the statements in this news release are forward looking statements and we caution our stockholders and others that these statements involve certain risks and uncertainties. Factors that may cause actual results to differ from expected results include fluctuations in commodity costs, the company's ability to integrate acquisitions and to realize the anticipated synergies and cost savings, the effects of competitive products and pricing, economic and political conditions that may impact customers' ability to fund purchases of our products and services, the company's ability to achieve the cost savings anticipated from cost reduction programs, fluctuations in foreign currency exchange rates, the timing of cash payments and receipts, end use demands for wireless communication services, the loss of one or more significant customers, and other business factors. Investors should also review other risks and uncertainties discussed in company documents filed with the Securities and Exchange Commission.
Andrew Corporation
News Media Contact:
Renato Graziano, +1 (708) 236-6620
publicrelations@andrew.com
or
Investor Contact:
Lisa Fortuna, +1 (708) 236-6507