Aurora Networks® (ANS) and RUCKUS® Networks are now Vistance Networks
The move will allow
Tomasz Zuranksi, CEO,
Features and Benefits of ARRIS HMC3021 Hybrid Set-Top Box
The HMC3021 is a next-generation set-top that has been designed to deliver HD content to basic subscribers. The low-cost set-top converts a service provider's digital signal within the home so that subscribers can view HD content, like VOD, without the need for a more expensive, traditional set-top box. This facilitates the migration of subscribers to IP-based services with little interruption or outward investment on the part of the service provider.
"With the analogue switch over in
Key features:
The ARRIS HMC3021 supports a wide range of video rates and decodes standard MPEG-2, H.264 and MPEG-4 transport streams including most audio/video formats. Additionally, it is designed to support different Conditional Access Systems (CAS). The set-top features include a standard SmartCard interface, flexible memory footprint, optional two-way Ethernet RJ-45 for interactive applications, and a 750 MHz processor.
- 750MHz, 1125 DMIPS CPU
- Digital video (64QAM/128QAM/256QAM)
- ITU-T J83 Annexes A/B/C compliant
- Single 54MHz to 1GHz digital video tuner
- 128Mb Flash memory
- 256Mb DDR3
- Accelerated 2-D graphics
- HDMI video output up to 1920 x 1080p
- HDCP digital copy protection
- Low power standby mode
- Multiple Condition Access System (CAS) support.
The HMC3021 Series became part of the ARRIS portfolio through the company's acquisition of Motorola Home. ARRIS combines world-class solutions for the entire video delivery chain by integrating innovative technologies across the cloud, network and home.
*
Visit our booth at ANGA COM @ Booths #K11 and #E21.
About
Group
About ARRIS
ARRIS is a premier video and broadband technology company that transforms how service providers worldwide deliver entertainment and communications without boundaries. Its powerful end-to-end platforms enable service and content providers to improve the way people connect – with each other and with their favorite content. The Company's vision and expertise continue to drive the industry's innovations, as they have for more than 60 years. Headquartered north of
ARRIS and the ARRIS Logo are trademarks or registered trademarks of ARRIS Enterprises, Inc. All other trademarks are the property of their respective owners. © 2013
SOURCE
Caroline Tarbett, +44 7914 014145, Caroline.Tarbett@arrisi.com; or Jeanne Russo, +1-215-323-1880, Jeanne.Russo@arrisi.com