Aurora Networks® (ANS) and RUCKUS® Networks are now Vistance Networks
CommScope (NASDAQ: COMM), a global leader in network connectivity, today announced the global availability of its evolved SYSTIMAX® Constellation® edge-based power and connectivity platform for today’s and tomorrow’s hyperconnected enterprises. Now compliant with virtually all applicable global power and data transmission standards, the system combines fault-managed power, hybrid power/data fiber and Constellation Points (CPs) in a star topology to connect hundreds or thousands of network devices and systems.
Compared to traditional structured cabling networks, the Constellation platform has a radically simplified star architecture that is modular and technology-agnostic. It supports AC and DC power applications and a variety of connectivity standards for IT/OT networks. Eliminating the need for a telecom room or wiring closet on every floor, it enables centralization of uninterruptable power supply (UPS) equipment, and CPs can now be deployed in ceilings, walls or equipment racks, using fewer components while supporting both converged and segmented networks.
Additionally, the Constellation platform delivers greater power and faster speeds to more devices, can slash installation labor by greater than 50% over traditional solutions, reduces space requirements and uses less plastic and copper to lower the network’s overall carbon footprint. The platform significantly extends service distances from equipment rooms and can deliver 10G and above speeds and 1kW fault-managed power to myriad connected devices in today’s increasingly dense urban environments.
“The Constellation platform enables our customers to support much denser urban centers and a proliferation of connected devices in their buildings,” said Luc Adriaenssens, VP, Building & Campus, CCS, CommScope. “By offering a modular, technology-agnostic solution, we’re giving our global customers more choices for building connectivity and power to the network edge—and helping them do it in a way that’s cost-effective, scalable and sustainable.”
About Constellation
The Constellation platform is part of CommScope’s award-winning SYSTIMAX® cabling and connectivity solutions portfolio. The platform consists of Propel™ fiber panels, power transmitters and power transition panels, which connect to CPs via patented hybrid power/data fiber trunks, and finally to devices using pre-terminated SYSTIMAX Cat 6A patch cords and cable assemblies.
By the numbers, the Constellation platform delivers:
· Up to 1800W power (across 110V/220 AC, 48V and 24V DC systems and PoE) to 250M effective transmission distance between equipment room and convergence points
· Up to 1000W power (across 110V/220 AC, 48V and 24V DC systems and PoE)) to 500M effective transmission distance between equipment room and convergence points
· Up to 700W power (across 110V/220 AC, 48V and 24V DC systems and PoE)) to 1000M effective transmission distance between equipment room and convergence points
· 10G bandwidth capabilities (or more, since it uses singlemode fiber as well)
· Up to 57% reduction in skilled installation labor hours
· Up to 50 devices supported per CP
· Up to 59% reduction in copper compared to traditional LAN
· Up to 65% less plastic used compared to traditional LAN
· Up to 40% less overall embodied network carbon
The evolved Constellation platform is available immediately worldwide. For more information, please visit the CommScope website.
—END—
CommScope and the CommScope logo are registered trademarks of CommScope and/or its affiliates in the U.S. and other countries. For additional trademark information see https://www.commscope.com/trademarks. All other product names, trademarks and registered trademarks are property of their respective owners.
About CommScope:
CommScope (NASDAQ: COMM) is pushing the boundaries of technology to create the world’s most advanced wired and wireless networks. Our global team of employees, innovators and technologists empower customers to anticipate what’s next and invent what’s possible. Discover more at www.commscope.com.
Follow us on LinkedIn and X. Sign up for our press releases and blog posts.
News Media Contact:
Luke Hamer
Luke.Hamer@commscope.com
Financial Contact:
Massimo DiSabato, CommScope
Massimo.Disabato@commscope.com
This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Source: CommScope