CommScope Addresses Challenges of Cell Densification In Capacity-Strained Wireless Networks

February 19, 2013 HICKORY, N.C.

To alleviate capacity concerns in their macro networks, many wireless operators are exploring or deploying lower power and smaller footprint cell sites. Often referred to as small cells, these applications—designed to increase overall sector density, or capacity—can present challenges when it comes to acquiring sites and integrating them into the macro wireless network.

Addressing these challenges, CommScope is adding its expertise in macro site deployment to multiple Andrew® RF cell densification solutions to create a portfolio of options that help operators address small cell deployment concerns.

“Crowded cell sites, zoning restrictions and RF engineering challenges make finding the right solution for adding network capacity with cell densification quite challenging for operators,” said CommScope’s Philip Sorrells, vice president of strategic marketing, Wireless. “Operators need options that can be tailored based on specific site requirements and deployed in a timely, cost-effective manner without disrupting service.”

In many urban and suburban areas, because the cost of acquiring a cell site can be greater than the cost of installing equipment, operators are looking to deploy lower power and shorter antenna cells (or mini-cells) that occupy less space. Operators often must aesthetically reduce the visual impact of their RF equipment to meet zoning and leasing requirements. Operators also must attend to engineering concerns such as minimizing interference with adjacent sectors and providing adequate backhaul to limit bottlenecking.

To address these challenges, CommScope’s versatile small cell solution portfolio includes:

  • The well-established ION®-M distributed antenna system (DAS), which the company has deployed for years in outdoor campuses of up to 20 kilometers in distance. “We view DAS as the original small cell platform for improving data throughput and quality of service for the subscriber,” said Sorrells.
  • Integrated concealment solutions that hide RF equipment in a monopole under one radome, which can be installed as standalone street poles or on existing structures. These concealed small cell solutions are customizable based on height and diameter, power output, sectorization and integrated Andrew RF equipment. All models are radio agnostic, meaning interoperable with existing radio equipment in multi-carrier environments with shared infrastructure.
  • Wireless backhaul support including the Andrew Sentinel™ Class 4 microwave antenna, now available in a compact and powerful 0.3 m (1 ft) diameter model. Sentinel antennas increase capacity through better spectrum reuse and longer deployment of higher modulation schemes, typically resulting in 40% higher network density. Groundbreaking radiation pattern envelopment offers superior interference immunity while sturdy design lends superior durability even in winds of up to 250 km/h (155 mph).
  • In North America, turnkey design, installation, project management and commissioning services plus a comprehensive RF Path warranty. CommScope plans to expand its turnkey small cell offerings in other regions later this year.

“You have to be flexible and creative to deliver small cell solutions that meet real-world deployment challenges,” said Sorrells. “CommScope is well-equipped with experience and a variety of product options to make small cell deployment a success for our customers.”

Related Blog Posts:

The Many Considerations For Small Cells

What Can History Teach Us About Small Cells?

Stuck In Line: Three Known Capacity Robbers Of Wireless Networks

Cast A HETnet Over Coverage And Capacity Networks

Andrew and ION are registered trademarks of CommScope, Inc. Sentinel is a trademark of CommScope, Inc.

About CommScope

CommScope (www.commscope.com) has played a role in virtually all the world’s best communication networks. We create the infrastructure that connects people and technologies through every evolution. Our portfolio of end-to-end solutions includes critical infrastructure our customers need to build high-performing wired and wireless networks. As much as technology changes, our goal remains the same: to help our customers create, innovate, design, and build faster and better. We’ll never stop connecting and evolving networks for the business of life at home, at work, and on the go.

This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

News Media Contact:
Wes Bates, CommScope
+1 972-952-9780 or publicrelations@commscope.com
or
Financial Contact:
Phil Armstrong, CommScope
+1 828-323-4848