ARRIS Launches First Gateway with ARRIS Secure Home Internet by McAfee®; Exclusively at Best Buy

July 12, 2017 America/New_York
ARRIS SURFboard® SBG7580-AC with ARRIS Secure Home Internet by McAfee delivers cybersecurity protection to devices in the home - including IoT devices - in a single product

SUWANEE, Ga., July 12, 2017 /PRNewswire/ -- ARRIS International plc (NASDAQ: ARRS) today launched the ARRIS SURFboard® SBG7580-AC cable modem gateway with ARRIS® Secure Home Internet by McAfee® exclusively* at BestBuy.com. A combination gigabit cable modem, Wi-Fi® router, Ethernet hub and home internet security center, the SBG7580-AC gateway is fast, secure, easy-to-use and eliminates monthly rental fees. As the first broadband gateway featuring McAfee's Secure Home Internet, the SBG7580-AC moves the security burden off your individual connected devices and onto your home internet's first point of entry for easier and better protection.

ARRIS SURFboard® SBG7580-AC with ARRIS Secure Home Internet by McAfee delivers cybersecurity protection to devices in the home – including IoT devices – in a single product

Cyberattacks in the connected home are a growing consumer concern. A recent McAfee study** revealed that 81 percent of consumers think it's important that their online identity and internet-connected devices are secure. As consumers install increasing numbers of connected devices into their home, savvy cybercriminals have morphed their focus to those new devices, knowing that many consumers fail to take the proper security precautions to protect themselves. Today, any device that connects to the internet is a potential target if not properly secured. This is why ARRIS partnered with McAfee, a leading independent cybersecurity company, to enable best-in-class security at the point where data flows in and out of the home.

Product Highlights

  • Ultimate Performance: Capable of blazing-fast gigabit speeds, the SBG7580-AC features a DOCSIS® 3.0 modem, 802.11ac Wi-Fi router and 4-port gigabit Ethernet hub in one product, making it ideal for whole families, avid streamers and downloaders, plus gamers who need a fast and reliable connection.
  • Connect and Protect – One Product and Protection For Your Devices: The SBG7580-AC has ARRIS Secure Home Internet by McAfee protection built right into the gateway, which means no additional software to install. As the entry point for the internet into the home, the SBG7580-AC can protect the devices connected to your network, by helping to stop malware, phishing, and more from reaching a connected device***, including your internet-connected appliances and products like smart thermostats, speakers and cameras. 
  • Easy to Use, More Control for Parents: According to a recent study from McAfee, 80 percent of parents are concerned with their children's online interactions. Thankfully, with the SBG7580-AC with ARRIS Secure Home Internet by McAfee®, it's never been easier or simpler to help protect your whole family from potential online threats.With automatic device discovery and profiling, there's minimal setup and no additional software installation required.The SBG7580-AC also offers comprehensive parental controls, allowing consumers to set custom access and controls by user and device profile, block children from accessing inappropriate content and pause internet access for a specific device or the whole network.
  • Savings: The SBG7580-AC eliminates monthly modem rental fees from internet providers, which can save as much as $120 a year. It also comes with three years of ARRIS Secure Home Internet by McAfee protection for free, an approximate $240**** savings.
  • Take Your Security with You: McAfee security doesn't end with your gateway. To extend the security benefits beyond your home network, all owners receive McAfee LiveSafe™ software, which provides antivirus, identity and privacy protection, free for 90 days. That means your PCs, Macs, smartphones and tablets stay protected with McAfee software whether you're at home or away. Learn more here.

"The ARRIS SBG7580-AC is the first gateway to incorporate device security into the gateway, the entry point for internet into the home. In doing so, we've created a single product that delivers cybersecurity protection to devices in the home, including unsecured IoT devices," said Sandy Howe, SVP and GM, Consumer Products Group at ARRIS. "Instead of installing and updating security software on every single connected device, now people can simply connect to protect. ARRIS pioneered gateway technology, and the SBG7580-AC with ARRIS Secure Home Internet by McAfee showcases our 20+ years of technology communications expertise."

"We pioneered the digital life protection space where we made it our mission to protect all the devices that our customers use," said John Giamatteo, Executive Vice President, Consumer Business Group at McAfee. "With the integration of Secure Home Internet into the ARRIS gateway, we are delivering on this mission with an industry leader. The best security software is the kind that people actually use, and together with ARRIS, McAfee is making it easier than ever for consumers to protect every connected device in the home."

Pricing and Availability
The ARRIS SURFboard SBG7580-AC with ARRIS Secure Home Internet by McAfee is available exclusively at BestBuy.com for $199.99.

About ARRIS
ARRIS International plc. (NASDAQ: ARRS) is a world leader in entertainment and communications technology. Our innovations combine hardware, software, and services across the cloud, network, and home to power TV and internet for millions of people around the globe. The people of ARRIS collaborate with the world's top service providers, content providers, and retailers to advance the state of our industry and pioneer tomorrow's connected world. For more information, visit www.arris.com.

For the latest ARRIS news:

ARRIS, the ARRIS Logo, and SURFboard are trademarks or registered trademarks of ARRIS Enterprises, LLC.  McAfee and the McAfee logo are trademarks of McAfee, LLC or its subsidiaries in the US and/or other countries. All other trademarks are the property of their respective owners.  © ARRIS Enterprises, LLC. 2017.  All rights reserved.

* Exclusively at Best Buy until Sept 30, 2017.

** In September 2016, McAfee commissioned OnePoll to conduct a survey of 9,800 consumers (aged 18-55+). Respondents were individuals who use an internet-enabled device on a daily basis in the following countries: Australia, Canada, France, Germany, Italy, Mexico, Netherlands, Spain, the U.K., and the U.S.

***ARRIS Secure Home Internet by McAfee blocks connected devices from reaching a known malicious site. As new and unknown sites are identified by McAfee, ARRIS Secure Home Internet by McAfee will automatically detect, block and secure connected devices from them.

****Actual rates may vary depending on a number of factors including, but not limited to: the services offered by cable service providers, network traffic, computer equipment, type of server, number of connections to server, and availability of internet router(s).An approximate value of $240 when compared to comparable offerings.

View original content with multimedia:http://www.prnewswire.com/news-releases/arris-launches-first-gateway-with-arris-secure-home-internet-by-mcafee-exclusively-at-best-buy-300486799.html

SOURCE ARRIS International plc

Jeanne Russo, +1 215.323.1880, jeanne.russo@arris.com; Kalia Farrell, +1.215.323.1059, Kalia.Farrell@arris.com